Input Trigger

This is an analyzer sequence parameter which specifies the type of trigger input which will cause the test set to start the acquisition.

Double-clicking in the Input Trigger field opens a dropdown list of the choices: